Labelled Data Modelling

Labelled Data Modelling involves creating predictive models based on datasets with predefined labels. These models are essential for supervised learning tasks like fault prediction.

Add a Supervised Fault Prediction Model

To add a supervised fault prediction model:

  1. Go to Genix Platform > Digital Apps Center > My Apps > APM Model Deployment and Configuration > Labelled Data Modelling.

  2. Choose either the Generic or Specific radio option:

    • Generic: Allows model creation applicable to multiple assets.

    • Specific: Creates a model tailored to an individual asset.

  3. Select an asset from the list.

  4. In the Failure Model List, select a failure mode relevant to the asset. By default, the first failure mode in the list appears at the top.

  5. Choose Supervised Fault Prediction as the model type.

  6. Click Add Model to initiate the model creation process.

    Labelled data modelling